Quectel EC200A 4G module PPP :chat -v -f pap, but Connect script failed, status = 0x1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Quectel EC200A 4G module PPP :chat -v -f pap, but Connect script failed, status = 0x1

953 次查看
sibingl
Contributor I

Issue log:

 pppd options in effect:
debug # (from /etc/ppp/peers/provider)
nodetach # (from /etc/ppp/peers/provider)
persist # (from /etc/ppp/peers/provider)
 dump # (from /etc/ppp/peers/provider)
noauth # (from /etc/ppp/peers/provider)
 user cmnet # (from /etc/ppp/peers/provider)
remotename cmnet # (from /etc/ppp/peers/provider)
 /dev/ttyUSB2 # (from /etc/ppp/peers/provider)
 115200 # (from /etc/ppp/peers/provider)
lock # (from /etc/ppp/peers/provider)
connect /usr/sbin/chat -v -f /etc/chatscripts/pap -T ******** # (from /etc/ppp/peers/provider)
 nocrtscts # (from /etc/ppp/peers/provider)
 local # (from /etc/ppp/peers/provider)
asyncmap 0 # (from /etc/ppp/options)
lcp-echo-failure 4 # (from /etc/ppp/options)
 lcp-echo-interval 30 # (from /etc/ppp/options)
 hide-password # (from /etc/ppp/options)
 ipparam cmnet # (from /etc/ppp/peers/provider)
 noipdefault # (from /etc/ppp/peers/provider)
defaultroute # (from /etc/ppp/peers/provider)
usepeerdns # (from /etc/ppp/peers/provider)
Sep 20 20:49:47 imx93-abb-chargedot pppd[293]: : # (from /etc/ppp/peers/provider)
Sep 20 20:49:47 imx93-abb-chargedot pppd[293]: noipx # (from /etc/ppp/options)

pppd 2.4.8 started by root, uid 0

Script /usr/sbin/chat -v -f /etc/chatscripts/pap -T ******** finished (pid 294), status = 0x1

Connect script failed

sibingl_3-1720428353245.png

 

 

In the .service file:

sibingl_0-1720427965136.png

Here is the modem_startup.sh:

sibingl_1-1720428079471.png

 

Here is the modem_startup_ppp.sh:

sibingl_2-1720428173023.png

 

If I manually excute the cmd on the console of the board: /etc/init.d/modem_startup.sh  ppp &,  the ppp0 card will be found and succeeds to ping internet.

But if the script /etc/init.d/modem_startup.sh  ppp & launched by .service file, the issue always exists, Connect script failed all the time.

 

I'm not clear what happend, pls help me out, thx

 

 

0 项奖励
回复
0 回复数