QN9090DK debug not starting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9090DK debug not starting

ソリューションへジャンプ
3,927件の閲覧回数
MikeCalm
Contributor II

Hi All,

I have issue with debugging using QN9090 dev kit. Most time when I start debug it can't find the hardware:

MikeCalm_0-1602519049731.png

Some LEDs flash and above popup is displayed.

The only thing I can do is disconnect from PC or randomly press RESET and ISP buttons on board and sometimes it allows to run.Most times not.

When it finally runs, debugger disconnects after a few minutes, and can't change breakpoints. Tried adding one and got this message:

MikeCalm_1-1602519545013.png

 

This befaviour is from new one.

Can anyone point to possible solution. Maybe it is faulty.

Thanks

Mike

ラベル(2)
0 件の賞賛
返信
1 解決策
3,895件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you are building the temperature sensor example and you are working on this, by any  chance, did you disable the low power configuration on the example ? Whenever you are using an example with the low power capabilities enabled you will lost the debugger functionality as it disable the pins in order to save power.

 

Could you please check the definition state of cPWR_UsePowerDownMode?

 

regards,

Estephania

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,896件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you are building the temperature sensor example and you are working on this, by any  chance, did you disable the low power configuration on the example ? Whenever you are using an example with the low power capabilities enabled you will lost the debugger functionality as it disable the pins in order to save power.

 

Could you please check the definition state of cPWR_UsePowerDownMode?

 

regards,

Estephania

 

0 件の賞賛
返信
3,882件の閲覧回数
MikeCalm
Contributor II

Hi Estephania,

Many thanks for help, it solved the issue.

Regards,

Mike

0 件の賞賛
返信
3,908件の閲覧回数
MikeCalm
Contributor II

Hi Estephania,

Thank you for help, but it didn't work..

Another observation. When I manage to start, when i click STOP icon, I have the error reported by target message (the second one in my first message).

And I am able to run much more often after pressing ISP and then RESET.

Is there anything else I can do?

Regards

Mike

0 件の賞賛
返信
3,915件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm that you loaded the ROM patch in this link ?

 

Please, let me know if that works for you.

 

regards,

Estephania

 

 

0 件の賞賛
返信