QN9090DK debug not starting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QN9090DK debug not starting

跳至解决方案
2,739 次查看
MikeCalm
Contributor II

Hi All,

I have issue with debugging using QN9090 dev kit. Most time when I start debug it can't find the hardware:

MikeCalm_0-1602519049731.png

Some LEDs flash and above popup is displayed.

The only thing I can do is disconnect from PC or randomly press RESET and ISP buttons on board and sometimes it allows to run.Most times not.

When it finally runs, debugger disconnects after a few minutes, and can't change breakpoints. Tried adding one and got this message:

MikeCalm_1-1602519545013.png

 

This befaviour is from new one.

Can anyone point to possible solution. Maybe it is faulty.

Thanks

Mike

标签 (2)
0 项奖励
回复
1 解答
2,707 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you are building the temperature sensor example and you are working on this, by any  chance, did you disable the low power configuration on the example ? Whenever you are using an example with the low power capabilities enabled you will lost the debugger functionality as it disable the pins in order to save power.

 

Could you please check the definition state of cPWR_UsePowerDownMode?

 

regards,

Estephania

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,708 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

I see that you are building the temperature sensor example and you are working on this, by any  chance, did you disable the low power configuration on the example ? Whenever you are using an example with the low power capabilities enabled you will lost the debugger functionality as it disable the pins in order to save power.

 

Could you please check the definition state of cPWR_UsePowerDownMode?

 

regards,

Estephania

 

0 项奖励
回复
2,694 次查看
MikeCalm
Contributor II

Hi Estephania,

Many thanks for help, it solved the issue.

Regards,

Mike

0 项奖励
回复
2,720 次查看
MikeCalm
Contributor II

Hi Estephania,

Thank you for help, but it didn't work..

Another observation. When I manage to start, when i click STOP icon, I have the error reported by target message (the second one in my first message).

And I am able to run much more often after pressing ISP and then RESET.

Is there anything else I can do?

Regards

Mike

0 项奖励
回复
2,727 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm that you loaded the ROM patch in this link ?

 

Please, let me know if that works for you.

 

regards,

Estephania

 

 

0 项奖励
回复