QN908x USB HID Generic interface on MAC OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN908x USB HID Generic interface on MAC OS

2,755 Views
kishans
Contributor III

Has any one tested QN908x HID USB interface on a MAC OS. When I tried it on MAC OS it doesn't seems to recognize, the same version of the HID USB example project works on the system which is loaded with Windows 10 OS. kindly let me know if there is any specific protocol support need to be added to make it working in MAC OS. Regards, kishan

0 Kudos
Reply
4 Replies

2,701 Views
kishans
Contributor III

ok @Ricardo_Zamora. 

Let me know if anyone else tested/ tried the NXP QN908x USB HID example application on a MAC OS, and if so please let me know the outcome.

-kishan

0 Kudos
Reply

2,734 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. We do not have examples that work with MAC OS. You can take the USB HID Generic example as a base, but you will need to adapt it to the needs and with the necessary features to make it work on that OS.

 

Regards,

Ricardo

0 Kudos
Reply

2,725 Views
kishans
Contributor III

Hi @Ricardo_Zamora ,

Thanks for the update, would like to know where can I look for the feature specification in order to make the QN908x USB HID work on MAC OS.

0 Kudos
Reply

2,711 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

For this information, you should go with that company, to get the USB specification to work with the OS of their machines.

 

Regards,

Ricardo

0 Kudos
Reply