QN908x USB HID Generic interface on MAC OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN908x USB HID Generic interface on MAC OS

2,762件の閲覧回数
kishans
Contributor III

Has any one tested QN908x HID USB interface on a MAC OS. When I tried it on MAC OS it doesn't seems to recognize, the same version of the HID USB example project works on the system which is loaded with Windows 10 OS. kindly let me know if there is any specific protocol support need to be added to make it working in MAC OS. Regards, kishan

0 件の賞賛
返信
4 返答(返信)

2,708件の閲覧回数
kishans
Contributor III

ok @Ricardo_Zamora. 

Let me know if anyone else tested/ tried the NXP QN908x USB HID example application on a MAC OS, and if so please let me know the outcome.

-kishan

0 件の賞賛
返信

2,741件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. We do not have examples that work with MAC OS. You can take the USB HID Generic example as a base, but you will need to adapt it to the needs and with the necessary features to make it work on that OS.

 

Regards,

Ricardo

0 件の賞賛
返信

2,732件の閲覧回数
kishans
Contributor III

Hi @Ricardo_Zamora ,

Thanks for the update, would like to know where can I look for the feature specification in order to make the QN908x USB HID work on MAC OS.

0 件の賞賛
返信

2,718件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

For this information, you should go with that company, to get the USB specification to work with the OS of their machines.

 

Regards,

Ricardo

0 件の賞賛
返信