QN9080 USB Dongle Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QN9080 USB Dongle Firmware

跳至解决方案
3,453 次查看
bmhuerta
Contributor I

Where can I find the latest firmware version for the QN9080 dongle? Apparently it should appear in the QTool installation directory, but I can not find it. I'm using the QTool Rev. 1.0.0, released on 2018-02-01.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,947 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi,

  The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup 

  To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive. 

-Anthony 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,948 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi,

  The new firmware is now available as part of the updated QTool installation package. It can be found in the "bin files" directory. https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup 

  To update the dongle firmware, short TP5 to ground (you can use the USB shield) and press the reset button. You should see a "CRP DISABLD" drive enumerate. Delete the firmware.bin file in that drive, and then drag-and-drop the new firmware.bin file into that drive. 

-Anthony 

0 项奖励
回复
2,947 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Borja,

  The QTool software is being updated very soon to include the firmware. I'll post back when the new version is available. 

-Anthony 

0 项奖励
回复