I run the prj_bass project, but it can not work.
I debug it with jlink, found that BLE stack APIs locate at the address around 0x01000000~0x0102000 (defined in fw_func_addr.h), but the content of the chip in the range is all 0xFF.
SDK version 1.4.0
The marking letter of chip is "9021 355Y5 00UMF"
I use the macro QN_9020_B4
解決済! 解決策の投稿を見る。
Hi,
What is the example that you are trying to run?
What are the lib that you have included?
Please look at the next AN https://www.nxp.com/docs/en/application-note/AN12288.pdf
Is it your custom board?
Regards,
Mario
Hi,
What is the example that you are trying to run?
What are the lib that you have included?
Please look at the next AN https://www.nxp.com/docs/en/application-note/AN12288.pdf
Is it your custom board?
Regards,
Mario
Thanks!
The example is QN902x_SDK_1.4.0\Projects\BLE\prj_bass.
I use the jlink commad in PRJROOT\src\link\iar\qn9020_flash.mac to get that the chip is “Device: QN9020 B3”.
After using the macro CFG_QN9020_B2, it works.
qn9020_flash.mac:
execUserReset()
{
__var chip_id;
chip_id = __readMemory32(0x40000088, "Memory");
if(chip_id == 0x2801) // QN9020 B0
{
__message "Device: QN9020 B0";
cfg_fw_9020_B0();
}
else if(chip_id == 0x2901) // QN9020 B1
{
__message "Device: QN9020 B1";
cfg_fw_9020_B1();
}
else if(chip_id == 0x2A01) // QN9020 B2
{
__message "Device: QN9020 B2";
cfg_fw_9020_B2();
}
else if(chip_id == 0x2B01) // QN9020 B3
{
__message "Device: QN9020 B3";
cfg_fw_9020_B2();
}
else if(chip_id == 0x2C01) // QN9020 B4
{
__message "Device: QN9020 B4";
cfg_fw_9020_B4();
}
else
{
__message "Error: unknown device ID: ", chip_id;
}
}