QN9020 SDK bug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9020 SDK bug

2,361 次查看
yijunma
Contributor II

#if (QN_SECURITY_ON)

int app_smpc_irk_req_ind_handler(ke_msg_id_t const msgid, struct smpc_irk_req_ind const *param,

                               ke_task_id_t const dest_id, ke_task_id_t const src_id)

{

    QPRINTF("IRK request indication idx is %d.\r\n", param->idx);

    uint8_t reject;

    uint8_t bonded_count = app_get_bond_nb();

    if (param->idx == 0xFF)

    {

        // We recognised this device, so update address for looking up correct LTK

        // It is no need to write back to NVDS.

        app_env.bonded_info[app_env.irk_pos - 1].peer_addr = app_env.dev_rec[param->idx].bonded_info.peer_addr;

        app_env.irk_pos = 0;

        return (KE_MSG_CONSUMED);

    }

param->idx == 0xFF

app_env.dev_rec[param->idx] will access out of boundary.

标签 (1)
0 项奖励
回复
1 回复

1,913 次查看
dougbrunner
Contributor I

It seems like the API is broken, at least in the case where multiple connections are allowed. AFAIK param->idx is supposed to identify the index of the active connection to which the IRK request applies, but when the remote device is recognized, 0xFF is passed instead, so the IRK request indication handler has no way of knowing which connection to get the peer address from. This bug bit me when I tried to connect from an iOS device that had been previously bonded: connections would repeatedly get set up and fail, with perhaps 100ms period, and after a few seconds of this the QN9021 would crash in a way I haven't been able to diagnose.

Since my application only needs to allow one connection at a time, meaning the correct connection index has to be 0, I implemented a workaround. Here's the patch for system/app/task/smp/app_smp_task.c:

@@ -312,6 +312,11 @@
  *
  ****************************************************************************************
  */
+
+#if BLE_CONNECTION_MAX > 1
+#  error "Workaround for https://community.nxp.com/thread/429593 can fail if more than one connection is allowed"
+#endif
+
 #if (QN_SECURITY_ON)
 int app_smpc_irk_req_ind_handler(ke_msg_id_t const msgid, struct smpc_irk_req_ind const *param,
                                ke_task_id_t const dest_id, ke_task_id_t const src_id)
@@ -325,7 +330,7 @@
     {
         // We recognised this device, so update address for looking up correct LTK
         // It is no need to write back to NVDS.
-        app_env.bonded_info[app_env.irk_pos - 1].peer_addr = app_env.dev_rec[param->idx].bonded_info.peer_addr;
+        app_env.bonded_info[app_env.irk_pos - 1].peer_addr = app_env.dev_rec[0].bonded_info.peer_addr;
         app_env.irk_pos = 0;
         return (KE_MSG_CONSUMED);
     }
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 项奖励
回复