QN9020 Advertising Period

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN9020 Advertising Period

3,066 次查看
tonyblake
Contributor I

Hi,

I'm new to the QN9020, can someone tell me how to set the advertising period of the device?

标签 (1)
0 项奖励
回复
3 回复数

2,892 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Tony,

Advertising is started with the app_gap_adv_start_req() function, where the last 2 parameters indicate the advertising interval min/max values. These values are normally set by the macros GAP_ADV_FAST_INTV1 and GAP_ADV_FAST_INTV2. The advertising interval goes in 625µs steps and can be in the range from 20ms (0x0020) to 10.24s (0x4000).

Regards,

Gerardo

0 项奖励
回复

2,892 次查看
tonyblake
Contributor I

Hi Gerardo,

Thank you for your reply. Are you saying that the maximum advertising interval can only ever be 10.24s? i.e. if scanning for a BLE device using a smartphone app the BLE device will only appear for 10.24s?

Tony

0 项奖励
回复

2,892 次查看
gerardo_rodriguez
NXP Employee
NXP Employee

Hi Tony,

If the advertising interval is set to 10s, it means that every 10s the device will send an advertising packet as long as the device stays in advertising mode. In this case, the scanning device (e.g smartphone), will detect the device every 10s. 

If you want to stop advertising, you can use the app_gap_adv_stop_req() function.

Regards,

0 项奖励
回复