Programmable BLE Central Receive Sensitivity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programmable BLE Central Receive Sensitivity

ソリューションへジャンプ
3,005件の閲覧回数
nidhintomy
Contributor IV

Hi All,

My HW setup is KW45 and SW setup is Central example.

In data sheet of KW45, -97.5 dBm is the receive sensitivity for 1Mbps.
Is it possible for us to change the receive sensitivity? Is there any API. 
If yes, please tell me, which document or api can be used for this purpose?

Best Regards,
Nidhin

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,995件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

元の投稿で解決策を見る

2 返答(返信)
2,996件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

2,929件の閲覧回数
nidhintomy
Contributor IV

Hi @Gavin_Jia ,

Thanks.

0 件の賞賛
返信