Programmable BLE Central Receive Sensitivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programmable BLE Central Receive Sensitivity

Jump to solution
2,901 Views
nidhintomy
Contributor IV

Hi All,

My HW setup is KW45 and SW setup is Central example.

In data sheet of KW45, -97.5 dBm is the receive sensitivity for 1Mbps.
Is it possible for us to change the receive sensitivity? Is there any API. 
If yes, please tell me, which document or api can be used for this purpose?

Best Regards,
Nidhin

0 Kudos
Reply
1 Solution
2,891 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

View solution in original post

2 Replies
2,892 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

2,825 Views
nidhintomy
Contributor IV

Hi @Gavin_Jia ,

Thanks.

0 Kudos
Reply