Power Amplifier/Low Noise Amplifier for 802.15.4 2.4 GHz MC13234

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power Amplifier/Low Noise Amplifier for 802.15.4 2.4 GHz MC13234

2,219件の閲覧回数
matthammond
Contributor I

I was wondering if Freescale offered an integrated RF Front End that might increase output power, receive sensitivity, and therefore range of its MC13234 wireless MCU. I noticed Texas Instruments offers the CC2592 2.4 GHz Range Extender for its products, and was wondering if Freescale has an analogous part that might be compatible with the MC13234. I don't see one offered, but maybe there is another solution that Freescale suggests that might compete with the +20 dBm output from the TI chip.

Thanks,

Matt

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,066件の閲覧回数
AngelC
Senior Contributor I

Dear Matt,

I am not familiar with TI’s CC2592 but there is a design developed by RFMD using the RF6555 and the MC1323x devices you may find useful. Please contact them directly for further details about the design.

Link: http://www.rfmd.com/content/zigbee%C2%AE-hansmartenergy-ami-6555mc1323

Regards,

AngelC

2,066件の閲覧回数
matthammond
Contributor I

Thank you, I will look into it!

0 件の賞賛
返信