Peripheral send rejection on update connection parameter after Master accepts it and send PARAM_REQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peripheral send rejection on update connection parameter after Master accepts it and send PARAM_REQ.

1,587件の閲覧回数
mahmoud_k_elkas
Contributor I

Hello everybody.

I'm using QN9080 as a peripheral, I implement connection parameter request using "APP_GapcParamUpdateCmd" API after Master accepts it and sends PARAM_REQ, peripheral send rejection on PARAM_REQ to master due to Collision. I read in specs that the master who sends rejection if there is any collision happens.

I have a couple of questions.

1- Why peripheral rejects that after master accepts?

2- I can catch the error code when the Master accepts/rejects the connection parameter.
    is there any way to catch the error code if peripheral sends it?

Any help?

pastedImage_2.png

ラベル(1)
  • QN

0 件の賞賛
返信
1 返信

1,514件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

How are you implementing the flow of the code to start the connection? Are you using some examples as a base? 

Regards, 
Estephania 

0 件の賞賛
返信