PN7160 RXN RXP interchangeablility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160 RXN RXP interchangeablility

2,641 Views
joka
Contributor I

Hi,

I am designing a NFC host controller (reader) board with PN7160, and would have a question on the antenna interface.

The antenna interface has pins RXN, TX1 TX2 and RXP that I am using. In the hardware design guide it tells me to connect RXN to TX2 through series capacitor and resistor, and the same for RXP to TX1. My layout with the chip package (PN7161A1EV/C100K) would prefer connecting RXN to TX2 and RXP to TX1. Could you confirm if this is OK or could it cause some issues with the reader functionality? As I see, the circuits are symmetrical, but maybe there is something withing the functions of TX1 and TX2 that forces me to use the recommended way?

Your recommendation in the HW design quide:

joka_0-1685438967678.pngjoka_0-1685438967678.png


My schematic at the moment:

joka_1-1685438992912.pngjoka_1-1685438992912.png

Thanks!

 

0 Kudos
Reply
2 Replies

2,605 Views
joka
Contributor I

Thank you very much Daniel!

0 Kudos
Reply

2,612 Views
danielchen
NXP TechSupport
NXP TechSupport

@joka 

 

This swap is not critical as the circuit is symmetrical.

You can use it also as TX2 connects to RXN, and TX1 connects RXP without any issue.

 

Regards

Daniel