PN7150 working without battery.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7150 working without battery.

Jump to solution
3,775 Views
dominusdrr
Contributor IV

Hi.

I'm developing a PCB circuit with a microcontroller and the NFC PN7150.

My hardware doesn't need a battery to work, so my question is:

Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?

I can't find any information on that subject, so it is assumed that there will always be a backup battery.

Any comment or suggestion is welcome

 

0 Kudos
Reply
1 Solution
3,763 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @dominusdrr .

Thank you for contacting NXP technical support.

 

>> Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?

Need to be connected to  a 5V source.

Please kindly refer to the 12.5.3.2 Configuration 2: supply connection in case a 5 V supply is used to generate RF field with the use of TXLDO of the datasheet as the link.

URL:https://www.nxp.com/docs/en/data-sheet/PN7150.pdf.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
3,764 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @dominusdrr .

Thank you for contacting NXP technical support.

 

>> Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?

Need to be connected to  a 5V source.

Please kindly refer to the 12.5.3.2 Configuration 2: supply connection in case a 5 V supply is used to generate RF field with the use of TXLDO of the datasheet as the link.

URL:https://www.nxp.com/docs/en/data-sheet/PN7150.pdf.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply
3,753 Views
dominusdrr
Contributor IV

Hi.

Thanks for your help.

0 Kudos
Reply