PN532 polling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,870件の閲覧回数
m3adn
Contributor I

Hi. 

I have a question regarding PN532.

Is there any way actually to make PN532 to poll/detect a card (let it be Mifare) without sending commands in loop like InListPassiveTarget but to receive an interrupt by IRQ pin whenever there is a card and only then proceed to receive the data?

I found that that later versions such as PN7120 / PN7150 support LPCD, which I think fits my requirements, but I'd need a confirmation to the fact that in order to retrieve any data from the card I should send a command and only then read the card.

I found this topic https://community.nxp.com/t5/NFC/How-to-generate-an-interrupt-to-the-processor-when-a-tag-is/m-p/589... talking about similar.

Any help is appreciated.

Ty.

タグ(4)
0 件の賞賛
返信
1 解決策
3,851件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. First of all, PN532 is a product that is not recommended for new designs.

I would recommend checking this Application Note. Please refer to section 3.3.

Also, I would recommend checking our PN7160 | NFC Controller with Integrated Firmware and NCI Interface.

 

Regards,

Ricardo

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,852件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. First of all, PN532 is a product that is not recommended for new designs.

I would recommend checking this Application Note. Please refer to section 3.3.

Also, I would recommend checking our PN7160 | NFC Controller with Integrated Firmware and NCI Interface.

 

Regards,

Ricardo

0 件の賞賛
返信
3,804件の閲覧回数
m3adn
Contributor I

Thank you Ricardo, as there is no other way to do it rather than sending the command to poll and waiting for response I consider this answered. 

One more question , is NCx3320 and NCx3321 already available on the market? And if so, it is possible to configure them without the NCI interface (I mean normal use of I2C or SPI)? 

I'm asking it cause the information about those chips is very limited.

Appreciate your help.

Daniel.

0 件の賞賛
返信