PN5190B2 RXP and RXN push-pull configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190B2 RXP and RXN push-pull configuration

Jump to solution
4,101 Views
Fion
Contributor I

Hi,

In PN5190B2 datasheet Figure 29. push-pull configuration,RXP connect to TX1 with C R and L,but in SPF-X-PNEV5190B_A1 (page7),RXP connect to TX2 with C and R, so which TX should RXP connect with?

0 Kudos
Reply
1 Solution
4,074 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fion 

This is a symmetrical design, RXN can be connected to TX1 or TX2, and the same goes for RXP. You can refer to the Demo design.

 

View solution in original post

0 Kudos
Reply
2 Replies
4,074 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Fion 

This is a symmetrical design, RXN can be connected to TX1 or TX2, and the same goes for RXP. You can refer to the Demo design.

 

0 Kudos
Reply
3,938 Views
Fion
Contributor I

Hi Kelly,

Another question, PN5190B2HN VFLGA40 footprint have 4 thermal pad in the corner, what should i do? connnect with GND or left float? Many thanks.

VFLGA40.png

0 Kudos
Reply