Nb Table List Count incorrect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nb Table List Count incorrect

3,823件の閲覧回数
13560436802
Contributor II

Hi, I have a problem.

1. There are four device in the Network, one coordinator, three router;

2. I use the PC software "ZGWUI.exe" send the command "Discover devices" to the coordinator device;

 The problem is that: the Nb Table List Count:2

 why the count is "2", but not "3"?

clipboard.png

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,670件の閲覧回数
13560436802
Contributor II

Hi Mario,

   1. 3 routers are joined to the coordinator directly;

   2. attachment is the log;

0 件の賞賛
返信

3,670件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

The received message that you are seeing is correct. You have to take as reference the index value.

In other words, the control bridge is only reporting the devices 0 and 1, the size of the packet for three entries (of the joined router) in the neighbor table cannot fit inside the same payload. So, you have to send the next command

01 02 10 4E 02 10 02 13 4C 02 10 02 10 02 11 03

The return values will be device 1 and device 2

Also, you can send the command through the raw data, general path.

pastedImage_1.png

The last byte is the index value

Regards,

Mario

0 件の賞賛
返信

3,670件の閲覧回数
13560436802
Contributor II

Hi Mario,

   Thank you very much. 

    Is there any other way to get the information about how many device in the network, and the device info?

    My purpose is about that ,the MCU(stm32)send a command to the bridge ask for the information about the network, 

    and the bridge reply the information ,include the number of device and each device  network address .

0 件の賞賛
返信

3,670件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

As you know the max size of Zigbee payload can only be 128 bytes which include Phy + MAC + NWK + APS header overload and routing related overhead and thus while forming the Mgmt LQI response, the NXP stack checks how many entries can fit and respond accordingly.  So, I recommend to increase the index if the entries are higher than 2 and send the management LQI request again.

Regards,

Mario

0 件の賞賛
返信

3,670件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

Thanks for the feedback, I am working with this issue with the developer's team.

I will get back to you with a feedback as soon as possible.

Mario

0 件の賞賛
返信

3,670件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

Could you please provide that sniffer log that you attached on your image?

Are the 3 routers joined to the Coordinator directly?

Regards,

Mario

0 件の賞賛
返信