NXH3670_BLE Audio application support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXH3670_BLE Audio application support

2,241 Views
pavan252
Contributor II

Hi

For my BLE audio application, NXP team suggested to use NXH series controller. Please find the below thread for earlier discussion.

###BLE Audio application support###

After checking the datasheet of NXH series i have below query

Can i use NXH3670 for multiple one to one connections simultaneously?

Because my Bluetooth device requires

1. BLE audio playback application from mobile and

2. Simultaneously it has to share the data from sensors connected to it to another slave device.

Can i use NXH for this application or do i need to use piconet or mesh applications?

Please suggest.

0 Kudos
Reply
1 Reply

2,202 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Pavan, I hope you're doing well!

 

The NXH3670 uses a proprietary 2.4GHz audio streaming extension to manage the audio portion of the system, requiring the use of both a dongle and a headset portion for a complete solution.

 

The proprietary wireless audio streaming protocol has been optimized for wireless gaming headset applications, providing high-quality forward audio streaming at low latency (<20ms) combined with a simultaneous voice microphone backchannel. Additionally, a wireless bidirectional data channel is available.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

0 Kudos
Reply