NTAG5 with PNEV7462C Board using NFC Cockpit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NTAG5 with PNEV7462C Board using NFC Cockpit

3,123 次查看
amighri
Contributor II

NTAG 5 Communication with PNEV7462C Board Using NFC Cockpit

I just started using PNEV7462C to read and write in NTAG5 Registers. In my first example i wanted to configure the GPIO_0 and GPIO_1 as Inputs. and As i read the Register A0 i expected that both GPIOs change the status. 

 The commands i used in Tx data without flags are as followed : 

C1A10022AF00 --> GPIO_Mode / plain Input 

C1A30C000000 --> GPIO_0 and GPIO_1 as Input

C0A00 -->  when i connect the GPIOs to Vcc (5v in this case i used a breadboard and some jumpers for this set up) the card response i get is : 03C80000 but I'm expecting 03D80000 ( GPIO1_IN_STATUS bit didn't change ) i tried many configurations like disabling the recievers , and use just the GPIO_1 as Input but the GPIO1_IN_STATUS bit in register A0 still don't change at all though I'm connecting it to Vcc. 

 

Can someone help me with this problem. 

 

Thank you in Advance. 

标记 (1)
0 项奖励
回复
3 回复数

3,081 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello,

I've checked this configuration using NTAG 5 NFC Cockpit GUI without any issues.

Please check the User Manual for NTAG 5 NFC Cockpit.

You will need to connect the PN7462 with the Cockpit firmware, and when opening the NTAG 5 Cockpit, you need to have both boards connected by USB and both antennas connected. Then the NTAG 5 Cockpit should open the configuration panel as shown in section 4; NTAG 5 NFC Cockpit GUI.

In the log panel you should see the next log, after a proper configuration:

 

 

> Writing configuration register PWMGPIO0:
NFC >> 22 C0 04 00 00 00 00 00 00 00 E0 39 00 
NFC << 00 0C 00 00 00 
Read configuration block 39h = 0C 00 00 00 
NFC >> 22 C1 04 00 00 00 00 00 00 00 E0 39 00 04 00 00 00 
NFC << 00 
Write configuration block 39h = 04 00 00 00 

 

 

After the configuration, you should be able to read the NTAG 5 with the PN7462 in the same NTAG 5 NFC Cockpit GUI and should get the next response at the log window.

 

> Reading configuration register PWMGPIO0:
NFC >> 22 C0 04 00 00 00 00 00 00 00 E0 39 00 
NFC << 00 04 00 00 00 
Read configuration block 39h = 04 00 00 00 

 

 

With this, you will have your GPIO0 configuration.

Please notice the next table for a better understanding of the frame sent:

22

Flag

C0

Read Config

04

Manuf ID

00

UID

00

UID

00

UID

00

UID

00

UID

00

UID

00

UID

E0

UID

39

PWM_GPIO_ CONFIG_0

00

 

 

I strongly recommend you that perform the configuration this way, before creating a full application using the PN7462

I hope this information may have been useful

Best Regards,
Fabian
0 项奖励
回复

3,057 次查看
amighri
Contributor II

Dear @Fabian_R 

Thank you very much for your detailedanswers it helped me a lot configuring the GPIOs. Just another question should be the NTAG5 power supplied in this case ? 

 

Thanks in advance.

Greetings,

0 项奖励
回复

3,042 次查看
Fabian_R
NXP TechSupport
NXP TechSupport

Hello!!

Yes, it should.

Best Regards,
Fabian
0 项奖励
回复