NTAG FD pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NTAG FD pin

1,751 次查看
schakoma
Contributor I

Hello. I'm using the NTAG I2C plus with Arduino pro mini. I need some help programming the FD pin to indicate to the reader that data is ready to be read from the I2C interface and if data has been read by the NFC interface. Thanks.

0 项奖励
回复
1 回复

1,677 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi schakoma:

 

The NTAG I2C plus has several triggering possibilities to provide input to a connected microcontroller to signal events on the RF interface. This signaling can be done through the Field Detection pin or through the equivalent registers over I2C.

danielchen_0-1650845914673.png

 

Please refer to AN11579: How to use NTAG I2C plus for bidirectional.

https://www.nxp.com.cn/docs/en/application-note/AN11579.pdf

 

 

Regards

Daniel