NTAG FD pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG FD pin

2,426件の閲覧回数
schakoma
Contributor I

Hello. I'm using the NTAG I2C plus with Arduino pro mini. I need some help programming the FD pin to indicate to the reader that data is ready to be read from the I2C interface and if data has been read by the NFC interface. Thanks.

0 件の賞賛
返信
1 返信

2,352件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi schakoma:

 

The NTAG I2C plus has several triggering possibilities to provide input to a connected microcontroller to signal events on the RF interface. This signaling can be done through the Field Detection pin or through the equivalent registers over I2C.

danielchen_0-1650845914673.png

 

Please refer to AN11579: How to use NTAG I2C plus for bidirectional.

https://www.nxp.com.cn/docs/en/application-note/AN11579.pdf

 

 

Regards

Daniel