NO Bluetooth connection once again!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NO Bluetooth connection once again!!

16,685 Views
ralphxyz
Contributor III

Rapid-IoT:

Yesterday I was at least getting prompted for a password now a P6E9D devic eis seen

but I do not get prompted for a password connection string.

Seems like someone programed this device and should be able to answer, most of the 

answers I have seen have been guesses " try 999999" or the like.

IMG_20190424_153441542.jpg

IMG_20190424_153426138.jpg

Thanks,

Ralph

Labels (1)
28 Replies

12,349 Views
i_beckmann
Contributor I

Try to „ignore the [bluetooth] device“ first on the device (e.g. smartphone) that prompts you for the password.

0 Kudos
Reply

12,349 Views
ralphxyz
Contributor III

Thank you Ingo for the reply! Boy this shows how ignorant I am of Bluetooth protocols.

How does one  „ignore the [bluetooth] device“??

I tried not entering a password if that is what you mean.

Seems like there should be an authoritarian person who actually knows what the password is,

unless these processors are programmed with AI, then I'd understand why no one knows what the device might use.

I am not even getting the password prompt now.

This device, NXP Rapid-Iot, certainly is not high on my list to recommend to anyone interested in learning about IoT.

Ralph

0 Kudos
Reply

12,349 Views
i_beckmann
Contributor I

Hey Ralph,

in iOS, go to "Settings", then "Bluetooth", then in the list of your BT devices select your Rapid IO gadget (could be "connected" or unconnected), then click on the info "i" on the right hand side, and finally do "ignore this device". Hope that helps!

0 Kudos
Reply

12,349 Views
ralphxyz
Contributor III

Thanks Ingo, the problem is no devices are being listed!!

also I have Android devices not iOS, wish I had a iOS device just for testing.

Anybody in the eastern Long Island, NY USA area with a iOS device I could test with?

I still would like the password, as I am sure I will eventually get this working.

If I cannot get a bluetooth connection how would I get a refund?

Ralph

0 Kudos
Reply

12,349 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Are you trying to connect with your device again and you are not able to find the rapid iot in your phone?

If this is the issue, please delete the device that you have added in your rapid iot studio.

Please let me know if you still have the issue.

Regards,

Mario

0 Kudos
Reply

12,349 Views
ralphxyz
Contributor III

Thank you Mario, the Rapid-IoT has never been connected with bluetooth, so it is not in the rapid-IoT studio!!

Occasionally I have seen a P6E9D on my phone bluetooth connection and on my computer but I do not know the password so I have never connected! I think I have to turn bluetooth off and reset then turn bluetooth on and reset

then I "might" see the P6E9D device but cannot connect!!

Ralph 

0 Kudos
Reply

12,349 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Could you please look at the next community post

https://community.nxp.com/thread/498190

Regards,

Mario

0 Kudos
Reply

12,349 Views
ralphxyz
Contributor III

Thanks Mario, that thread is about connecting apps with bluetooth and USB.

I am not connecting an app just trying to connect the device through Bluetooth!

I have tried using a app but since the device is not connected it does not work!

If I reset the device I see the bluetooth device P6E9D, I do not know if that is the Rapid-IoT device.

If that is the Rapid-IoT device what is the password?

Ralph

0 Kudos
Reply

12,347 Views
ralphxyz
Contributor III

Mario I got a email from you but it returns a broke link.

RE: What is the example that you are using?

I am not using any example!

could you please delete the devices that you have added in the rapid IoTpage.

I have not added any devices in the rapid IoTpage!

Could you please try to connect the device after that 

I am trying!!

Ralph

0 Kudos
Reply

12,347 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

You have the right version. Could you please flash the rapid again.

https://community.nxp.com/docs/DOC-342913

I want to discard the firmware software that is pre-flashed.

Please let me know your findings.

Regards,

Mario

0 Kudos
Reply

12,347 Views
ralphxyz
Contributor III

Thanks Mario, using Windows 10 I do not have a USB connection so I cannot flash!!

Of course I also do not have a Bluetooth connection in Windows 10!

I will setup a RaspberryPI possible that will see the device.

Ralph

0 Kudos
Reply

12,347 Views
ralphxyz
Contributor III

I tried pressing all 4 buttons at the same time and have the flashing orange led.

But still no USB connection, now what?

Ralph

0 Kudos
Reply

12,347 Views
ralphxyz
Contributor III

I did a hard reset of the device which restored things.

I tried using a Raspberry Pi. I see the P6E9D device in Bluetooth but do not have the Password!

I do not see any indication that the USB is detected, running lsusb I see:

Bus 001 Device 004: ID 0461:4dd7 Primax Electronics, Ltd

Bus 001 Device 007: ID 046d:c03d Logitech Mouse

Bus 001 Device 006: ID 0424:7800 Standard Microsystems Corp.

Bus 001 Device 003: ID 0424:2514 Standard Microsystems Corp. USB 2.0 Hub

Bus 001 Device 002: ID 0424:2514 Standard Microsystems Corp. USB 2.0 Hub

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

If I unplug the USB cable from the device I get the same result so the Rapid-IoT device is not being detected on the Raspberry Pi or on Windows 10!

How do I get a replacement or refund?

Ralph

0 Kudos
Reply

12,347 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Could you please try with another PC? If the PC detects the device, could you please flash again.

Please accept my apologies, the device is facing has some flash issues.

Could you please follow the warranty process?

Returns and Warranty Information

Regards,

Mario

0 Kudos
Reply

12,347 Views
ralphxyz
Contributor III

Hi Mario, thanks for the help!! I tried another Windows 10 computer and a Raspberry Pi, no USB I have a Windows XP Pro I'll try that.

Two questions:

Is the P6E9D device I am seeing while attempting bluetooth connection the Rapid-IoT device?

If so what is the Bluetooth password? Possible bluetooth will work, it would be great to be able to flash the device 

but if bluetooth works I could at least still use the device.

Ralph

0 Kudos
Reply

12,344 Views
ralphxyz
Contributor III

Unbelievable!!

I have a USB connection using Windows XP Pro!! Of course windows says there is a problem with the hardware,

I see a DATALINK drive with a Details text file and a HTML file MBED.

I do not know if I will be able to flash the device.

Do I just copy the .bin file to the DAPLINK drive?

Ralph

0 Kudos
Reply

12,344 Views
ralphxyz
Contributor III

Darn I "think" I am seeing the Hexiwear docking station not the Rapid-IoT device.

When I plug the device directly in I do not see it in File Explorer.

What is the bluetooth password?

Ralph

0 Kudos
Reply

12,344 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Ralph,

Are you using the Rapid IoT Application?

pastedImage_1.png

What is the complete process that you are following?

Regards,

Mario

0 Kudos
Reply

12,344 Views
ralphxyz
Contributor III

I had tried the Rapid Iot Application but did not see any devices!

So I was trying just to connect to the device using standard bluetooth connection from my phone to the device

as you normally connect bluetooth devices. That failed also.

Eventually after multiple tries and resets soft and hard I eventually saw the P6E9D device.

I could not connect for lack of a password.

Now that I can see the P6E9D device I am try to use the Rapid IoT application.

It appears to be connecting BUT the output does not change the light sensor does not change when I cover up the device, the direction sensor output does not change when I move the device!!

The computer Cloud application shows the device which I select but it has no data!

Rapid IoT.png - Google Drive 

Rapid IoT 1.png - Google Drive 

Ralph

0 Kudos
Reply

12,344 Views
ralphxyz
Contributor III

On my phone using the Rapid IoT application when I select the device there is a flashing bluetooth icon in the lower right corner of the screen this flashes for a while then the data from the various sensors appears and the flashing icon stops flashing. The icon never flashes again the data is not updated!!

Ralph

0 Kudos
Reply