NFC NHS3152

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC NHS3152

3,146 Views
keesdehaan
Contributor I

#

What is the NFC load impedance of the NHS3152? 20 or 80 ohm

Is there a EMC filter inside the NHS3152 chip ?                                                                                                                    What is the Copt matching capacitor  ?                                                                                                                                  Is total capacitance  50 pf + Copt ?                                                                                                                                        Can you give some guideline to match the NFC antenna

Greetings Kees de Haan

Labels (1)
1 Reply

3,021 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kees,

The NHS3152 is an NFC transponder, it has no reader capability. Therefore no EMC filter is necessary on the LA/LB pins.


The internal chip capacitance at the antenna inputs is 50pF. The impedance of the antenna should be such that is resonates slightly above 13.56MHz. This can be achieved by careful matching of the antenna inductance or in case of a too low inductance by adding an external capacitor across the antenna (pF range).
Please look at the https://community.nxp.com/docs/DOC-341105 for a nice explanation of the antenna design process.

Passive programming of the firmware of the NHS3152 is not supported.

Regards,

Mario