NCF3320 NCJ3320 data sheet differnce

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NCF3320 NCJ3320 data sheet differnce

2,344件の閲覧回数
lim
Contributor II

can i know why do you separate  NCF3320 and NCJ3320 with temperature range? 

 

Data sheet contents of NCJ3320 cannot be found in NCF3320. Are the functions not available in NCF3320?

 

NCJ3320 product sheet

 

8.7.2.21 T4RloadHi register

~

8.7.2.23 T4CounterValHi register

 

Receiver configuration

8.17.3 RxSynchValH register

~

8.17.5 RxSynchMod register

0 件の賞賛
返信
1 返信

2,333件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

As the device you are using is under NDA and as it is used for automotive applications you will need to go with your DBM (Distributor Business Manager)  for further support on this matter as we do not have access to the information. Sorry for the inconvenience may cause.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信