Missing DK6Programmer.exe?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing DK6Programmer.exe?

ソリューションへジャンプ
9,241件の閲覧回数
Alsanie
Contributor I

Hello,
I am trying to follow the example:
https://www.nxp.com/document/guide/getting-started-with-the-k32w061:GS-K32W061

 

which build the example and flash it. But I can't find the tool "DK6Programmer" anywhere.

ラベル(4)
0 件の賞賛
返信
1 解決策
9,223件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Alsanie,

 

You can find the DK6 Production Flash Programmer installer in the SDK (Path: SDK_2_6_4_K32W041ADK6\tools\JN-SW-4407-DK6-Flash-Programmer).

The Install Location by default will be "C:\NXP\DK6ProductionFlashProgrammer\".

Hope this helps.

 

Regards,

Ricardo

元の投稿で解決策を見る

3 返答(返信)
6,155件の閲覧回数
SpecialCodeMaster
Contributor I

hello,

i have a problem with loading my file . bin using usb to my pcb  i installed the application dk6 programmer i defined my usb in pc by zigbee gateway user interface  i followed the tutorial video for it in k32061 with jn5189  i connect the usb and i made the following commands 

1-DK6Programmer = he gave me that the dk6 is defined in my cmd

2-DK6Programmer.exe -l = he gave my port number for my usb (COM5)

3-DK6Programmer -s COM5 -P 500000 -e FLASH -Y -p MyFile.bin = he gave me error opening connection

why he give me that in fact in the zigbee gateway user interface when i pressed open port and then startNWK he gave me that like he send data for the usb but in the received message section there is no response. can you help me?

0 件の賞賛
返信
9,224件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Alsanie,

 

You can find the DK6 Production Flash Programmer installer in the SDK (Path: SDK_2_6_4_K32W041ADK6\tools\JN-SW-4407-DK6-Flash-Programmer).

The Install Location by default will be "C:\NXP\DK6ProductionFlashProgrammer\".

Hope this helps.

 

Regards,

Ricardo

9,212件の閲覧回数
Alsanie
Contributor I

Than you!

0 件の賞賛
返信