MRB-KW01 debug connection ???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRB-KW01 debug connection ???

2,407 Views
martinw
Contributor III

A query on the MRB-KW01 eval board.

Is it possible to debug using the USB port?

I was told that there was a debugger present on the eval board.

Regards

Martin Wakely

0 Kudos
Reply
1 Reply

2,255 Views
PBH
NXP Employee
NXP Employee

The short answer is no - sorry.

The USB connector is used for serial over USB communication via a pre-programmed USB2SER MCU.

To debug the MKW01 you will need to use a USB to JTAG debug cable like the P&E Multilink FX via

J5 the SWD connector (10 way pin header) on the MRB. These are orderable on the Freescale website -

Universal Multilink FX High-Speed Development|Freescale

I hope this helps.

Pete

0 Kudos
Reply