MMG3014NT1 matching circuits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMG3014NT1 matching circuits

1,886 Views
shashankmutha
Contributor I


Hello,

    We intend to use the MMG3014NT1 between 400 and 410MHz. May I ask you to please provide the input and output matching circuits for the same.

Thank you for your time,

0 Kudos
Reply
1 Reply

1,703 Views
jasonchiang
NXP Employee
NXP Employee

Below solution is tuned to 460MHz CW for reference.

pastedImage_0.png

pastedImage_6.png

Part
 

Value

Vendor Part #

C1, C4

100 pF

CQM1885C1H101JB01 Murata

C2

10 pF

CQM1885C1H100JB01 Murata

C3

                 1.8 pF

CQM1885C2A1R8CB01 Murata

C5

                7.5 pF

CQM1885C1H7R5DB01 Murata

C6

                0.1 uF

GRM21BR71H104A01L Murata

C7

               2.2 μF

C0805C225J4RAC Kemet

L1

               7.5 nH

0603CS-7N5XJL
 
Coilcraft

L2

56 nH

0805CS-560XJL
 
Coilcraft

L3

11 nH

0603CS-11NXJL
 
Coilcraft

R1

0 Ω

ERJ3GEY0R00V Panasonic

Q1

MMG3014NT1