MCU Peripheral Wiki

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU Peripheral Wiki

2,114件の閲覧回数
ignisuti_
Contributor IV

I was at the Freescale Technology Forum this year and heard mention of a peripheral wiki. Is this complete? If so, where is it? If not, when will it be complete?

I see a ton of features/peripherals in the Kinetis Reference Manuals. Although there are high level descriptions in there about the peripheral, I still don't have a clear understanding of when each one would be useful.

A good example of this are the timers. I'm currently using a KW2x MCU that has FlexTimers, Period Interrupt Timers, and Low Power Timers. The Periodic Timer has thus far done everything I needed it to do, but I keep thinking maybe one of the others would have some feature that would be better. A quick reference guide would greatly help me make those sort of decisions.

タグ(1)
0 件の賞賛
返信
1 返信

1,860件の閲覧回数
AngelC
Senior Contributor I

Hello Joe,

The MCU peripheral wiki is still under development and there is no exact date of release. In the mean time, you may refer to the Kinetis Peripheral Module Quick Reference for an overview of Kinetis K modules. These are very similar to KW2x family and might help clarifying your doubts. For KW2x code examples you may download BeeKit Wireless Connectivity Toolkit.

Link: http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf

Regards,

AngelC

0 件の賞賛
返信