MC33814

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33814

1,689 Views
berniecheah
Contributor I

Hi,

 

I would like to check if the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter? We are using a 5V buffer at the moment because we do not want to risk it.

Tags (2)
0 Kudos
Reply
1 Reply

1,490 Views
reyes
NXP TechSupport
NXP TechSupport

I’m afraid that it is not possible to connect the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter, the reason is that the Digital interface input of the MC33814 is dependent from VCC voltage and VCC voltage should be 5V. Using a level shifter is the best solution for this case.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply