MC33814

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33814

1,691件の閲覧回数
berniecheah
Contributor I

Hi,

 

I would like to check if the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter? We are using a 5V buffer at the moment because we do not want to risk it.

タグ(2)
0 件の賞賛
返信
1 返信

1,492件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

I’m afraid that it is not possible to connect the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter, the reason is that the Digital interface input of the MC33814 is dependent from VCC voltage and VCC voltage should be 5V. Using a level shifter is the best solution for this case.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信