MC13213 and SCI problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213 and SCI problem

1,776 Views
dawnulric
Contributor I

I am working with MC13213 and try to get some message to send, but when I check the message through sniffer I found they were incorrect. There were others mixed in them and after a while MC13213 would not send any more.I have tried checking my program under debug model, oddly it works well. I really have no idea about that and wonder why. I also want to ask where can I find more detailed information about MC13213 and its SCI register stuff. It seems that its datasheet which I download from the web is not useful enough.

0 Kudos
Reply
1 Reply

1,710 Views
soledad
NXP Employee
NXP Employee

Hi, 

I would recommend you to use a lower baudrate in order to discard any issue in software that is making the device to miss some data.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply