License for Zigbee / BeeStack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License for Zigbee / BeeStack

ソリューションへジャンプ
5,849件の閲覧回数
ming_
Contributor I

Hi, I'd like to know the License Fee of Zigbee and BeeStack.

Is necessary to have the License? If yes, what is the cost?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,010件の閲覧回数
AngelC
Senior Contributor I

Dear Min,

BeeStack (Freescale’s ZigBee stack) is completely free of charge and could be obtained from BeeKit Wireless Connectivity tool. No license is required to use it at all.

Beekit: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT

However, and due to its code size, a proper IDE/compiler license should be obtained (if you do not have one already) to compile and load the BeeStack applications.

Regards,

AngelC

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,011件の閲覧回数
AngelC
Senior Contributor I

Dear Min,

BeeStack (Freescale’s ZigBee stack) is completely free of charge and could be obtained from BeeKit Wireless Connectivity tool. No license is required to use it at all.

Beekit: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT

However, and due to its code size, a proper IDE/compiler license should be obtained (if you do not have one already) to compile and load the BeeStack applications.

Regards,

AngelC

0 件の賞賛
返信
5,010件の閲覧回数
ming_
Contributor I

Thanks for Quick respond

Really amazing to me the Freescale doesn't charge abut BeeStack !!

If I build own product with BeeStack, which is use Zigbee protocol, Still we don't have to pay license fee to Zigbee alliance? 

If I build own product with Home Automation Application of BeeStack, it can talk to other vendor's End Point or Router ?

0 件の賞賛
返信
5,010件の閲覧回数
AngelC
Senior Contributor I

Dear Min,

It basically depends on whether you want your product to be ZigBee compliant (with the ZigBee Logo) or not. If you do not want your product to be ZigBee Compliant, you do not need any license or certification to sell it, but you cannot put the ZigBee logo on it.

Moreover, the BeeStack solutions have been tested to interoperate with other vendor’s ZigBee devices, so if you base your solution in any of our projects, it is likely to be interoperable too. However, it will depend in the other devices’ settings such as security and profile used.

Regards,

AngelC