Kinetis KW01 codeexample for radio in KDS 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis KW01 codeexample for radio in KDS 3

2,186 Views
andreaswickströ
Contributor I

Hi

Is there any codeexample running the radio for KDS 3 using GCC compiler?

Best regards

Andreas

Labels (1)
0 Kudos
Reply
3 Replies

1,857 Views
luisburgos
NXP Employee
NXP Employee

Hi Andreas,

Unfortunately KW01 connectivity software is not supported in KDS.

At this moment, IAR is the only IDE which supports this software.

You can find the connectivity software in www.freescale.com/mrb-kw0x webpage, in the downloads tab, protocol stacks section:

Modular Reference Boards for Kinetis KW0x

protocol.png

Make sure to first install KSDK 1.2.

Best regards,

Burgos.

0 Kudos
Reply

1,857 Views
andreaswickströ
Contributor I

Hi

Is there any extra documentation in how to use the code with KDS. What files to include and how to use them?

Are there any plans to implement the radiostack to SDK packet for KDS for easy use with KDS?

Best regards

Andreas

Från: luisburgos

Skickat: den 13 augusti 2015 22:43

Till: Andreas Wickström <aw@awes.se>

Ämne: Re: - Kinetis KW01 codeexample for radio in KDS 3

<http://jiveon.jivesoftware.com/mpss/c/8AA/PDcDAA/t.1pj/DLlo1vb4TIOqz0giBjJKlA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

Kinetis KW01 codeexample for radio in KDS 3

reply from Luis Antonio Burgos Lopez <http://jiveon.jivesoftware.com/mpss/c/8AA/PDcDAA/t.1pj/DLlo1vb4TIOqz0giBjJKlA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSm0DCfK-2FoBRlib7qNpPojL6SBiWX1g4GR7Oy31lISJ6po2ST5JTY7b0tC3q1eRz5M-3D> in Wireless Connectivity - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/8AA/PDcDAA/t.1pj/DLlo1vb4TIOqz0giBjJKlA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTFn-2FSzQpBPfvjl8khTgTDBi2SoreSGXVJ8MKbt3hG783j-2B2ZB6zPooh4hq12Ji3Yk-3D>

0 Kudos
Reply

1,857 Views
luisburgos
NXP Employee
NXP Employee

Hi Andreas,

Yes, there are plans to implement the connectivity software stacks for KDS at the beginning of 2016.

Regarding to the documentation you mentioned, we don´t have support on that yet.

Best regards,

Burgos.

0 Kudos
Reply