KW45B41Z-EVK custom application development

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KW45B41Z-EVK custom application development

264 次查看
sreevishakh
Contributor II

Hi Team, 

I am using the KW45B41Z-EVK board. I have a few questions; can you please support me?

1. Please provide the link for the sample application and application notes to to start with the KW45 EVK board

2. Is it possible to flash a custom application in KW45 micro? What will be the interface for flashing the application into micro?

3. Will the NXP IoT mobile application source code be available to download?

 

Best regards,

Sreevishakh

 

0 项奖励
回复
2 回复数

255 次查看
luis_maravilla
NXP Employee
NXP Employee

Hello Sreevishakh

I would recommend starting with the Getting Started with the KW45B41Z Evaluation Kit | NXP Semiconductors instructions.

Download the latest SDK version [25.06] from the MCUXpresso SDK Builder

The Interface to test the SDK examples is the MCUXpresso IDE tool [latest version 25.06] as described in the getting started guide, then you can test any SDK examples with the KW45 EVK board.

Please refer to the following link for more detailed instructions Run a demo using MCUXpresso IDE — MCUXpresso SDK Documentation

If you want to start testing some applications related to Wireless and Bluetooth please to refer to the Bluetooth Low Energy Demo Applications User’s Guide , this guide describes the hardware and toolchain requirements and steps to build and run the demo applications examples included in the software development kit. The examples are located in the SDK Wireless_examples->bluetooth folder

If you need some other information as Application notes, User Manuals, datasheets etc please refer to KW45B41Z-EVK Main page Documentation section.

For testing any custom application, I would strongly recommend you take an existing example from the SDK as a base and then apply the modifications to your custom requirements; The Interface for flashing is the same MCUXpresso Tool.

The Source code for NXP IoT Toolbox app is not available for download or review.

Best Regards

Luis

0 项奖励
回复

245 次查看
sreevishakh
Contributor II

Hi Luis maravilla,

Thank you very much for your valuable inputs. It will really help me to proceed working with the KW45 development board.

 

Best regards,

Sreevishakh

 

0 项奖励
回复