KW45 external RC RESET circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 external RC RESET circuit

1,008 Views
Lingyinglu
Contributor I

Hi guys

     I design wireless key base on BLE KW45 chip,I have some questions,please support,TKS.

1.for the Reset pin23,Whether external RC RESET circuit is required?if need the RC,how long is the reset time?

2.for the Program pins SWD-CLK&SWD_DIO,Whether the external pull up or pull down is required?

 

 

0 Kudos
Reply
1 Reply

980 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Lingyinglu ,

 

Hope you are doing well!

1. An external RC reset circuit is not required. But if you added it, a common RC reset time is 10-20 ms. Should not be less than 2 μs.

2. External pullup resistors are recommended for the SWD pins to prevent them from floating.

 

Best regards,

Gavin

0 Kudos
Reply