KW41 marking code issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41 marking code issue

2,804 Views
seanwu
Contributor V

Dear sir,

 

KW41 marking code issue as below the first word (9) of 2nd line is different with NXP AN5377 shown L as below pictures.

Can you help to check what is the different between “9” & “L” ?

pastedImage_4.png

pastedImage_5.png

Thanks.

BR,

Sean Wu

Weikeng

Labels (3)
Tags (2)
0 Kudos
Reply
3 Replies

2,559 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

on the AN5377 is just a sample, the L can be different number depending the part that you are using, I believe that you are using the MKW41Z512VHT4

I hope this will help you.

regards

Vicente Gomez

0 Kudos
Reply

2,559 Views
seanwu
Contributor V

Dear Sir,

Could you please explain what the number mean? What does "9" mean?

And I also see the number is "L" on FRDM_KW40Z. What does "L" mean?

Is there another number?

pastedImage_1.png

Thanks.

BR,

Sean

0 Kudos
Reply

2,559 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

the L is on the KW40 

9 is for KW41

there are more number or letter for different MCU familys

Regards

Vicente Gomez

0 Kudos
Reply