KW38 debug via PEmicro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW38 debug via PEmicro

2,431 Views
LISI1
Contributor I

HI, At present, when developing KW38, we have encountered problems of burning and debugging. Errors are as follows

ide:MCUXpresso IDE v11.9.1_2170

1717749916113.png1717749955547.png1717750135082.png

 

Looking forward to your reply, thank you.

0 Kudos
Reply
3 Replies

2,329 Views
LISI1
Contributor I

Thank you, the issue has been resolved, will be closed

0 Kudos
Reply

2,374 Views
Itzel_UV
NXP Employee
NXP Employee

Hello,

 

I will be helping you in this case,

 

I notice that you have 2 questions with the topic involving the KW38, by any chance are they related? I that case, the communication will be at this same thread for practicality.

 

Could you confirmed if you're using a same custom board?

kw38 debug failure via external jlink - NXP Community

 

Regards,

Itzel

 

0 Kudos
Reply

2,386 Views
LISI1
Contributor I
Can you help me with that? Thank you
0 Kudos
Reply