KW38 debug by PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW38 debug by PE

Jump to solution
2,423 Views
LISI1
Contributor I

HI,

 ide:MCUXpresso IDE v11.9.1_2170

I would like to ask a question. At present, when using KW38 chip to develop ble project, we have encountered problems of burning and debugging. Errors are as follows

 

LISI1_0-1718073767530.png

 

LISI1_1-1718073767813.png

 

LISI1_2-1718073767542.png

 

 

Looking forward to your reply, thank you.

0 Kudos
Reply
1 Solution
2,406 Views
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 3 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

View solution in original post

0 Kudos
Reply
2 Replies
2,365 Views
LISI1
Contributor I

It's a problem with our board,thank you

0 Kudos
Reply
2,407 Views
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 3 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

0 Kudos
Reply