KW38 - BLE central and peripheral simultaneously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KW38 - BLE central and peripheral simultaneously

跳至解决方案
4,849 次查看
dawid_kasieczka
Contributor III

Hello, I'm using FRDM-KW38 board for BLE purposes. SDK version is 2.6.6 and MCUXpresso v11.1.1. I'm trying to create application that works as peripheral (advertises and is connectable) and scan at the same time, connecting to another peripherals. Is it possible with this MCU and SDK? I looked through provided examples but didn't find anything that fits my GAP structure idea. If it's possible, how I can achieve it? 

标签 (2)
0 项奖励
回复
1 解答
4,775 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Dawid, I hope you're doing well!

 

It's possible to change the GAP role of the device, maintain current connections, and then form a new connection using the new GAP role. This can be observed when using the Wireless UART SDK example for the FRDM-KW38 by following this procedure:

Two FRDM-KW38 devices and a mobile phone with the IoT Toolbox App are needed for this procedure.

  1. Program both FRDM-KW38 devices with the Wireless UART SDK Example (…\SDK_2.6.6_FRDM-KW38\boards\frdmkw38\wireless_examples\bluetooth\w_uart)
  2. Change the role on FRDM board A to GAP Peripheral and start advertising.
  3. Connect to FRDM board A using the IoT Toolbox phone app.
  4. Change the role on FRDM board A to GAP central and start scanning. Change the role on FRDM board B to GAP peripheral, and start advertising.
  5. Now both the phone and FRDM board B should be connected to FRDM board A.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

在原帖中查看解决方案

2 回复数
4,776 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Dawid, I hope you're doing well!

 

It's possible to change the GAP role of the device, maintain current connections, and then form a new connection using the new GAP role. This can be observed when using the Wireless UART SDK example for the FRDM-KW38 by following this procedure:

Two FRDM-KW38 devices and a mobile phone with the IoT Toolbox App are needed for this procedure.

  1. Program both FRDM-KW38 devices with the Wireless UART SDK Example (…\SDK_2.6.6_FRDM-KW38\boards\frdmkw38\wireless_examples\bluetooth\w_uart)
  2. Change the role on FRDM board A to GAP Peripheral and start advertising.
  3. Connect to FRDM board A using the IoT Toolbox phone app.
  4. Change the role on FRDM board A to GAP central and start scanning. Change the role on FRDM board B to GAP peripheral, and start advertising.
  5. Now both the phone and FRDM board B should be connected to FRDM board A.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

4,776 次查看
dawid_kasieczka
Contributor III

Thanks for the answer! That what I was exactly looking for. I modified it slightly to scan and advertise at the same time and it worked. That's good enough base for development of my app.

0 项奖励
回复