KW36: Why Write Response not sent for Write request?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36: Why Write Response not sent for Write request?

1,870件の閲覧回数
skalyan2
Contributor IV

Hi,

I am facing a issue in KW36 in sending Write response command. In my case is that my mobile app is trying to enable Client Characteristic Configuration Descriptor(CCCD) for a characteristic in my gattdb, but when the app sends Write Request for the writing the CCCD, the NXP stack doesn't send the Write Response sometimes for that.

Because of this my app disconnects from the KW36, 30 seconds after the Write Request is sent(I assume this is because of supervision timeout in phone/app)

I have attached the airtrace in which I have bookmarked my issue.

Regards,

Sai Kalyana Raman

ラベル(3)
0 件の賞賛
返信
1 返信

1,762件の閲覧回数
xing_chang
NXP Employee
NXP Employee

Hi [email protected]‌,

Your HID device is mouse or keyboard, maybe the operating system took over the control of HID, so you can't operate it.

0 件の賞賛
返信