KW30Z gHardwareParameters reserved data usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW30Z gHardwareParameters reserved data usage

1,820 Views
lucianfiran
Contributor V

IAR 7.50;  KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0)

What is the usage of  reserved[42] data, what module use this data ?

For backward compatibility with what ?


framework\Flash\Internal\Flash_Adapter.h

typedef PACKED_STRUCT hardwareParameters_tag
{
  uint8_t  reserved[42];             /* for backward compatibillity */
    uint8_t  ieee_802_15_4_address[8]; /* IEEE 802.15.4 MAC address */
    uint8_t  bluetooth_address[6];     /* Bluetooth address */
    uint32_t xtalTrim;                 /* KW4x only */
    uint32_t edCalibrationOffset;      /* KW01 ED offset */
    uint32_t pllFStepOffset;           /* KW01 fine tune pll */
    uint32_t gInternalStorageAddr;     /* The start address of the internal storage used for OTA update.
                                          A value of 0xFFFFFFFF means that the External storage is used. */
}hardwareParameters_t;

framework\Flash\Internal\Flash_Adapter.c

/* Hardware parameters */
hardwareParameters_t gHardwareParameters;

This data occupies quite some RAM and ROM.

0 Kudos
Reply
1 Reply

1,702 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Lucian

This reserved memory is used to keep the data structure. All the APIs in the Flash_Adapter.c uses this structure, so it shouldn't be changed. Accordign to the Reference Manual

Some members of this structure may be ignored on a specific board/silicon configuration. Also, new members may be added for implementation specific purposes and the backwards compatibility must be maintained.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply