KW01 UI question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW01 UI question

1,471 Views
cwchen14
Contributor I

Hi, I founded an exe file named "KW01_Connectivity_Software.exe" on the official website of NXP, is that a UI used for KW01?

If the answer is not, where could I download the UI?

Does the UI use for free?     

0 Kudos
Reply
1 Reply

1,431 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Sean, I hope you're doing well!

 

The KW01's connectivity software is a collection of different drivers and example code developed for this MCU. When executing the file, it will install the SDK and some example projects to the specified path. These projects can be opened and edited using the IAR Embedded Workbench IDE.

 

For more information, there's some documentation included in the installation directory, inside the "doc" folder, covering different topics like development process and stack explanations.

 

Please let me know if you have any further questions.

 

Best regards,

Sebastian

0 Kudos
Reply