K32W FTDI interface can't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32W FTDI interface can't work

2,127件の閲覧回数
danieltseng
Contributor V

I use "LPC-Link2" for debugging can work, but it doesn’t work when I use "FTDI".

FTDI : JP4&JP7 short 2 and 3.

PC's USB connection Carrier Main Board show following:

pastedImage_1.png

Use MCUXpresso IDE to download, it will not download

pastedImage_2.png

ラベル(1)
  • KW

2 返答(返信)

2,047件の閲覧回数
danieltseng
Contributor V

Hi Mario,

I already understand, no wonder I can't try it out.

Thanks.

Daniel

2,047件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Daniel,

The FTDI is not for debugging purposes.

We provide a tool, DK Production Flash Programmer can be used to program the binary files into the DK006 boards. The installation of this tool is described in DK6 Production Flash Programmer Installation.


This tool provides a faster program process without an external debugger, it uses a serial interface.

Regards,

Mario