JN518x flash programming protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN518x flash programming protocol

Jump to solution
6,358 Views
usaygo
Contributor III

Hello,

Is there any document of flash programming protocol between PC and JN5189?

Previously the document "JN51xx bootloader operation" does explain it. Now JN5189 seems to have very different protocol.

0 Kudos
Reply
1 Solution
6,345 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please check the chapter 38 of RM.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
5,931 Views
usaygo
Contributor III

Just for reference, I picked up the simpler commands sequence to write data onto FLASH of JN518X.

//Seigo

Command Bytes Sequence:
0000094E00A709AE19
^1^^^2^3^4^^^^^^^5
1: always zero
2: size of the sequence (including all bytes, bigendian)
3: command id (0x4E=Open ISP)
or response id
4: command parameters (depending on commands)
or response parameters (the first byte always its command status, success or error code)
5: CRC32 (from 1: to 4:)

===
Firstly set ISP pin as LO and RESET module,
The connect UART port as 115200bps 8N1.

>0000094E00A709AE19
Command ID=4E(PARAMETERS:00): Unlock ISP
<0000094F00BE129F58
Command RESPONSE=4F(PARAMETERS:00): Unlock ISP(00:Success)

>00000832214A0494
32(): Get Device Info
<000011330088888888CC0000148DDBB66D
33(0088888888CC000014): Get Device Info(00:success, 88888888:chip id, cc000014:version)

>0000194E01112233445566778811223344556677884B1703XX
4E(0111223344556677881122334455667788): Unlock ISP(01: Start ISP, 1122...88:Key)
<0000094F00BE129F58
4F(00): Unlock ISP(00:Success)

--- If you try to change baud, you can call the command of Set Baud Rate here (0x27,0x28 command).

>00000A40000F3E5AD196
40(000F): Open Memory for Access(00:FLASH, 0F:Mode=RdWrErEa)
<00000A410000AF27A630
41(0000): Open Memory for Access(00:Success, 00:Handle=0)

>0000124200000000000000420000CCA2F324
42(00/00/00000000/00420000): Erase Memory(00:Handle, 00:Mode(always 0), 00000000:Address=0x0, 00420000:Size=0x2400=97KB)
<000009430012A7D054
43(00): Erase Memory(00:Success)

>000012440000000000000042000024173967
44(00/00/00000000/00420000): Blank Check Memory(00:Handle, 00:Mode(always 0), 00000000:Address=0x0, 00420000:Size=0x2400=97KB)
<000009450044FD77D2
45(00): Blank Check Memory(00:Success)

--- here, transmit firmware binary file (.bin) from the top without skipping any bytes.
--- note: the transmit chunk must be 512bytes (= FLASE sector size).

>0002124800000000000000020000...
48(00/00/00000000/00020000/...data...):
Write memory(00:Handle, 00:Mode(always 0), 00000000:addr=0x0, 00020000:length=0x200=512B, ...)
<0000094900E84838DE
49(00): Write memory(00:Success)

>0002124800000002000000020000...
48(00/00/00020000/00020000/...data...):
Write memory(00:Handle, 00:Mode(always 0), 00020000:addr=0x200, 00020000:length=0x200=512B, ...)
<0000094900E84838DE
49(00): Write memory(00:Success)

>0000094A00C3656B1D
4A(00): Close Memory(00:Handle)
<0000094B00DA7E5A5C
4B(00): Close Memory(00:Success)

>00000814F3478169
14(): Reset
<0000091500FE462A86
15(00): Reset(00:Success)

 

0 Kudos
Reply
5,999 Views
peter111
Contributor I

I got it, reference manual

0 Kudos
Reply
6,000 Views
peter111
Contributor I

Can you please tell me what RM is referring to?

0 Kudos
Reply
6,346 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please check the chapter 38 of RM.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
6,341 Views
usaygo
Contributor III

Hi,

Thanks! That's what I wanted!!! I didn't notice the information is in RM.

0 Kudos
Reply