JN5189 application problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5189 application problems

1,582件の閲覧回数
jack_huang1
Contributor IV
The application of JN5189 is as follows: 1. JN5189 supports hibernation, can you set different RAM areas for power-down and retention?If yes, can you provide relevant documentation? 2. The SDK version used is SDK_2.6.2_JN5189.By capturing the packet, we can see that when sending data, only the short address of the sending node is carried in the packet. Now we hope that the packet can carry the short address and MAC address of the sending node simultaneously, and the receiver can resolve the short address and MAC address information of the sender in the packet. How to achieve this function?Do we have any proposals to recommend?Thank you very much!
0 件の賞賛
返信
1 返信

1,558件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @jack_huang1,

I hope you are doing great.

1. Please look at the power down example that we provide in the SDK.

/* Keep All SRAM banks for warm boot */

            config.pm_config |= PM_CFG_SRAM_ALL_RETENTION;

2. I am not sure if I am following your question. Do you want to send in the payload the short address and the mac address?

I think the next API could help you to request the mac address of the node zps_eAplZdpIeeeAddrRequest

If you already have the short address.

 

Regards,

Mario

0 件の賞賛
返信