JN5189 Config memory restoring

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5189 Config memory restoring

8,168件の閲覧回数
Marcin1
Contributor II

Hello,

For reasons that I will wirte about in another post, I erased Config memory on JN5189 using DK6Programmer and now I cannot communicate with with device using DK6Programmer

I would like to ask for way to restore this memory, please.

 

Marcin

ラベル(1)
  • JN

0 件の賞賛
返信
10 返答(返信)

8,152件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

What is the command that you used to erase that specific memory?

The JN5189 provides a bootloader in ROM that could help you with this setup.

What is the command that you are typing?

Could you please type the next command?

DK6Programmer.exe -s COM11 -h

mario_castaneda_0-1638312965771.png

Regards,

Mario

0 件の賞賛
返信

8,144件の閲覧回数
Marcin1
Contributor II

Hi @mario_castaneda ,

Thank you for fast response.

I used command:

DK6Programmer.exe -s COM11 -e Config

Every command with DK6Programmer.exe -s COMx for chip with erased Config memory i got:

Error opening connection: Read error

Response after -h command:

Error po erase Config memory.png

 

 

Regards,

Marcin

0 件の賞賛
返信

8,111件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Could you please try to press the ISP button before you type the command?

However, is it possible that you could try to program the device using the MCUxpresso using CMSIS or Jink?

Regards,

Mario

 

 

0 件の賞賛
返信

8,081件の閲覧回数
Marcin1
Contributor II

Hi, @mario_castaneda 

I can not program my device using MCUxpresso.

Sorry but it is also not that simple to press ISP button in my system.

Is there any other options to fix it?

If not I will try to press ISP button but it makes me to put a lot of effort.

Regards,

Marcin

 

8,007件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Did you get the previous Config information?

DK6Programmer.exe -s COM11 -r Config

some parameters (trimming parameter) are written in our factory, they would necessarily be different so you could expect problems in the radio behavior if we write different ones.

Please do not erase the Config information.

Regards,

Mario

0 件の賞賛
返信

7,994件の閲覧回数
Marcin1
Contributor II

Hi @mario_castaneda ,

Thank you for your response.

I'm sorry, but I can not get previous Config information from that chip. I can get it from other chip if it's needed.

The problem is that -s function does not work for that chip.

Is there any other option to write data besides DK6Programmer -s COMx function?

Regards,

Marcin

0 件の賞賛
返信

7,980件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Please do not erase the config file.

I highly suggest that must not erase the CONFIG page, and for the erased device, if you do not save the previous information the device is can not be recovered because it needs some parameters from our factory.

What config values that you want to modify?

Regards,

Mario

0 件の賞賛
返信

7,901件の閲覧回数
Marcin1
Contributor II

Hi @mario_castaneda 

I would like to know if there is way to somehow write new config values into Config memory.

I do not know which values i need to modify. I suppose that I need to write all of them.

Regards,

Marcin

0 件の賞賛
返信

7,891件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Marcin,

I look if there is a way to reprogram the CONFIG values.

I highly suggest you that must not erase the CONFIG page.

Unfortunately, the erased device is bricked. Each device has different CONFIG values preprogrammed in our manufacture.

Sorry for any inconvenience that this may cause you.

Regards,

Mario

8,028件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

I am checking the problem that you have. The command erases the complete config information and the tool needs that information for programming purpose.

I am checking if there is a way that you could reprogram some values in this case.

Please do not type this command again.

Regards,

Mario