JN5179:Load Binary File into Flash Memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5179:Load Binary File into Flash Memory

1,876 Views
wupengfei
Contributor II

1) Failed to read chip details on COM3

2) $ JN51xxProgrammer.exe  -s COM3 -f AN1180_154_HomeSensorCoord_JN5168.bin

       reading chip ID -check cabling and power

0 Kudos
Reply
1 Reply

1,596 Views
davidashraf
Contributor V

Hello wupengfei‌

Follow these connections when flashing 
-> Make sure you connect RX of programmer ->TX of module and vice versa 
-> VDD of module -> 3.3v ( not higher or lower ) 
-> GND of module -> ground
-> SPIMISO -> Ground 
-> RESET -> Ground then 3.3v and then leave it on 3.3v


Also Make sure the driver for your serial programmer is installed correctly 

Flashing now should succeed 
after it's done make sure you return SPIMISO pin to 3.3v before doing a RESET else the code will be removed ( this might have been you're problem ) 

I hope this help
Let me know if it worked for you

Regards 
David 

0 Kudos
Reply