JN5169 programming connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5169 programming connections

3,044 次查看
pierrelgcb
Contributor III

Hello,

I plan to use JN5169-001-M00-2Z modules as end devices without any carrier PCB. I am thinking about a programming solution.

1 - Does a hardware programming tool exist ? I mean, hardware connect the module inside the tool. Flash the module. Disconnect the module from the tool.

2 - Does a connector reference exist for the module form factor ?

3 - Programming datasheet tells to connect UART0 pins. Can I only connect RX/TX ? Or RTS/CTS are needed too ?

Thanks for your help. Regards.

Pierre

3 回复数

2,247 次查看
pierrelgcb
Contributor III

Not so easy to discover NXP ZigBee world. Good getting started web pages are ZigBee 3.0|NXP and Support Resources for JN516x MCUs|NXP .

1 & 2 - No hardware prog tool, neither connector found in documentations. I will build it.

3 - Ref Des DR1174 links RX/TX/RTS/CTS.

0 项奖励
回复

2,247 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Pierre,

You can also look at the next community post.

https://community.nxp.com/thread/460072 

Regards,

Mario

2,247 次查看
pierrelgcb
Contributor III

Hi Mario,

thanks for the link. I will receive hardware soon and start playing with.

Regards,

Pierre