JN5169 not support the clustered that 0x0001 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5169 not support the clustered that 0x0001 ?

736 次查看
Janson
Contributor I

Using  ZWGUI, add an emergency button to the zigbee network ,using read attribute command to  get athe remaining battery power. The log window returns no data, but the Wireshark packet capture tool shows that there is data returned and it is parsed as the Zigbee protocol POWER CONFIG.

ZWGUI,

3.jpg

 

 

 

 

wireshark tools:

1.png

The question 2.  INTRUDER ALARM SYSTEM (0X0501) not support

the log view in ZWGUI can not receive data when press down the SOS button, but the Wireshark tool can capture it. 
2.png

so, how can I get the data 

0 项奖励
回复
1 回复

705 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Maybe this community post could help you:ZigBee 3.0 Adding cluster on KW41Z - NXP Community. It is for another device, but a similar procedure should be done.

 

Also, we highly recommend moving to the JN5189 Wireless MCU for Zigbee® and Thread, as is our focus part for ZigBee/Thread. It is supported by our MCUXpresso IDE and MCUXpresso SDK. There are several SDK examples, like driver examples (GPIO, UART, SPI, I2C), RTOS examples, and Wireless examples (ZigBee and Thread).

 

If you are looking for a multiprotocol MCU, then I would recommend the K32W061/41 or the K32W041AM/A.

 

Best Regards,

Ricardo

0 项奖励
回复